:MEASure:EYE:ERATio:SOURce

Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Eye
Waveform type:
NRZ

Command Syntax

:MEASure:EYE:ERATio:SOURce  {CHANnel{N} | DIFF{1:8}{A|C} | CGMemory{1:8} | FUNCtion{1:16} | WMEMory{1:8}}

{N} identifies a specific channel and must be selected from {1:8}{A|B|C|D}. For example, 3C.

Query Syntax

:MEASure:EYE:ERATio:SOURce?

Description

Selects the source waveform on which to perform the ERATio measurement.