:MEASure:EYE:PAM:RMS
Command Syntax
:MEASure:EYE:PAM:RMS
Query Syntax
:MEASure:EYE:PAM:RMS?
Description
Starts Eye/Mask mode's PAM4 Level RMS measurement, which measures the "thickness" of a selected level of a PAM4/6/8 eye diagram. On NRZ signals, the thickness of both level zero and one are measured. Select the actual level to be measured using the :MEASure:EYE:PAM:RMS:LEVel child command. To measure all the levels on a signal, you must send this command once for each level as there is no command for simultaneously measuring all levels. The query form of the command returns the measured value. Sources can be any displayed PAM or NRZ waveform from a channel, differential channel, color-grade memory, or function. For example, CHAN1A, CGMemory1, or FUNCtion1.
Measurement Identification
Avoid subtle programming errors! To ensure that the correct measurement is installed or queried, always explicitly identify a measurement when installing a measurement or querying a measured value, status, or detail. To identify a measurement, specify the measurement's source waveform (:SOURce child command). With some measurements, you may also need to specify other identifying values. Generally, when selecting a measurement using FlexDCA's GUI, if a dialog appears prompting you to select values, you should explicitly specify these values when remotely identifying the measurement. More information.
For example, to return the status of the measurement, :MEASure:EYE:PAM:RMS
flex.write(':MEASure:EYE:PAM:RMS:SOURce CHAN1A')
if flex.query(':MEASure:EYE:PAM:RMS:STATus?') == 'CORR';
measurement = flex.query(':MEASure:EYE:PAM:RMS?')
else:
details = flex.query(':MEASure:EYE:PAM:RMS:STATus:DETails?')
reason = flex.query(':MEASure:EYE:PAM:RMS:STATus:REASon?')
Related Commands
| Command | Equivalent Setting in PAM-N Analysis Setup Dialog |
Description |
|---|---|---|
:MEASure:PAM:EYE:ESTiming
|
Receiver Sample Timing | Configures the timing for sampling the signal data for all PAM measurements in Eye/Mask mode. Depending on measurement conditions, this command may not affect the measurement. |
:MEASure:PAM:EYE:ELMethod
|
Eye Center Location | Selects the basis for determining the location of an eye's center on the waveform: at maximum eye width or maximum eye height. Depending on measurement conditions, this command may not affect the measurement. |
:MEASure:PAM:EYE:PPERcent
|
Eye Level Width | Defines the timespan (in percentage of symbol width) over which an eye's amplitude level is measured. |
:MEASure:PAM:EYE:TIME:LTDefinition
|
Time of Level | Specifies the method used to locate the time at which to measure an eye's level. |
:MEASure:PAM:AMPLitude:UNITs
|
Amplitude Units | Sets the amplitude units for measurement: volts, Watts, or percent. |
This Eye mode measurement can be applied to both NRZ and PAM waveforms.
Requires FlexDCA revision A.04.50 and above.
Example Command Sequence
:SYSTem:MODE EYE :CHAN1A:SIGNal:TYPE:AUTO OFF // Specify signal type, if needed. :CHAN1A:SIGNal:TYPE PAM4 :SYSTem:AUToscale :MEASure:EYE:PAM:RMS:SOURce CHAN1A :MEASure:EYE:PAM:RMS:LEVel LEVel2 // Select logic level to be measured. :MEASure:EYE:PAM:RMS // Measure and return value. :MEASure:EYE:PAM:RMS?