:MEASure:TDR:USER:CFILe:CLEar
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Package License:
L-RND
L-SNT
Command Syntax
:MEASure:TDR:USER{1:8}:CFILe:CLEar
Description
Removes an existing configuration file for a user measurement. This removes the measurement from TDR mode's User toolbar. A user measurement is created using the :MEASure:TDR:USER:CFILe parent command.
Use the :MEASure:TDR:USER parent command to turn on the measurement and return the measured value.
Requires FlexDCA revision A.05.00 and above.