:MEASure:TDR:USER:REGion
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Package License:
L-RND
L-SNT
Command Syntax
:MEASure:TDR:USER{1:8}:REGion {DISPlay | REGion{1:8}}
Description
Selects a waveform measurement region over which to perform the user measurement. This allows you to restrict the measurement over a specific portion of the waveform over the X axis. Measurement regions are available in FlexDCA's Oscilloscope and TDR/TDT modes. Use the :MEASure:REGions:STATe command to turn on an configure measurement regions.
Requires FlexDCA revision A.05.00 and above.