:MEASure:TDR:USER
Command Syntax
:MEASure:TDR:USER{1:8}
{1:8} selects one of eight possible user measurements.
Description
Turns on the selected TDR mode user-defined measurement. The query form of the command returns the measured value. If the selected user measurement has not been created using the :CFILe child command, the value NaN (9.91E+37) is returned.
Requires FlexDCA revision A.05.00 and above.
Measurement Ready?
To confirm that the measurement is ready to read, you can query the measurement's status:
if ('CORR' in Flex.query(':MEASure:TDR:USER:STATus?')):
measurement = Flex.query(':MEASure:TDR:USER?')
If averaging is turned on (:ACQuire:AVERaging), you can also confirm if the measurement result is ready by comparing the number of specified averages (:ACQuire:ECOunt?) versus the number of measurement sweeps that have occurred (:MEASure:TDR:USER:COUNt?). The technique uses the :COUNt? common measurement query. For example,
if (Flex.query(':MEASure:TDR:USER:COUNt?') >= Flex.query(':ACQuire:ECOUNt?')):
measurement = Flex.query(':MEASure:TDR:USER?')
You can also use an acquisition limit lest to test that a number of waveform samples, or pattern acquisitions have completed before returning a measurement. Refer to the :LTESt:ACQuire:CTYPe command.
Common Measurement Child Queries
This command supports the use of the following common measurement queries: :LOCation?, :COUNt?, :MAXimum?, :MINimum?, :MEAN?, and :SDEViation?.
Measurement Identification
Avoid subtle programming errors! To ensure that the correct measurement is installed or queried, always explicitly identify a measurement when installing a measurement or querying a measured value, status, or detail. To identify a measurement, specify the measurement's source waveform (:SOURce child command). With some measurements, you may also need to specify other identifying values. Generally, when selecting a measurement using FlexDCA's GUI, if a dialog appears prompting you to select values, you should explicitly specify these values when remotely identifying the measurement. More information.
For example, to return the status of the measurement, :MEASure:TDR:USER
flex.write(':MEASure:TDR:USER:SOURce CHAN1A')
if flex.query(':MEASure:TDR:USER:STATus?') == 'CORR';
measurement = flex.query(':MEASure:TDR:USER?')
else:
details = flex.query(':MEASure:TDR:USER:STATus:DETails?')
reason = flex.query(':MEASure:TDR:USER:STATus:REASon?')
Child commands for measurement identification:
:MEASure:TDR:USER:SOURce:MEASure:TDR:USER:REGion