:MEASure:TDR:USER:CFLoaded?
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Package License:
L-RND
L-SNT
Query Syntax
:MEASure:TDR:USER{1:8}:CFLoaded?
Query Response
{1 | 0}
Description
Queries the existence of the specified user measurement. Returns a one if the measurement is defined and a zero it the measurement has not been setup.
Use the :MEASure:TDR:USER parent command to turn on the measurement and return the measured value.
Requires FlexDCA revision A.05.00 and above.