:MEASure:TDR:USER:COMMents?
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Package License:
L-RND
L-SNT
Query Syntax
:MEASure:TDR:USER{1:8}:COMMents?
Description
Returns the comment string for the selected user measurement. The comment string is defined in the measurement's XML definition file using the <Comments> tag. The comment string is limited in length to 512 characters.
Use the :MEASure:TDR:USER parent command to turn on the measurement and return the measured value.
Requires FlexDCA revision A.05.00 and above.