:MEASure:THReshold:EREFerence
Meas. mode:
Eye
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:MEASure:THReshold:EREFerence {TBASe | OZERo}
Query Syntax
:MEASure:THReshold:EREFerence?
Description
Sets the reference used to when establishing custom threshold definitions.
- TBASe
- Selects custom levels based on Vtop (100%) and Vbase (0%). When
TBASeis selected, use the:MEASure:TBase:METHodcommand if you want to define custom the top and base levels. - OZERo
- Selects custom levels based on one and zero levels.
This command is available in Eye/Mask mode only.
Example Command Sequence
:SYSTem:MODE EYE :MEASure:THReshold:EREFerence OZERo