:SPRocess:CTLequalizer:FZP

Instrument:
N1000A
N109x
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Package License:
L-RND

Command Syntax

:SPRocessN:CTLequalizer:FZP <low-frequency zero-pole>

<low-frequency zero-pole> is a double.

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:SPRocessN:CTLequalizer:FZP?

Description

Specifies the low frequency zero/pole applied by an IEEE based CTLE operator. The frequency is specified in Hertz. You can also set the Zero frequency (:CTLequalizer:ZERo), low frequency gain (gDC) (:CTLequalizer:GDC), and Pole frequency (:CTLequalizer:POLe).

Before selecting this command, send the :FUNCtion:FOPerator CTLE command to first create the operator followed by :CTLequalizer:DEFinition IEEE to define the type of CTLE.

Commands Available for Defining a CTLE Operator
Child Commands Description CTLE Definition Argument
POLE2 POLE3 GAIN2
:SPRocess:CTLequalizer:DEFinition Selects type of CTLE ■ ■ ■
:SPRocess:CTLequalizer:GAIN DC gain ■ ■
:SPRocess:CTLequalizer:GAIN:NORMalize Turns DC gain on or off ■ ■
:SPRocess:CTLequalizer:GDC Low frequency gain (Gdc and Gdc2) ■
:SPRocess:CTLequalizer:ZERo Zero frequency ■ ■ ■
:SPRocess:CTLequalizer:FZP Low-frequency zero/pole ■
:SPRocess:CTLequalizer:POLe Pole frequency ■ ■ ■
:SPRocess:CTLequalizer:PNOise Noise processing ■ ■ ■
:SPRocess:CTLequalizer:PRESets Recall and save CTLE settings as preset ■ ■ ■

For Reference Rx operator, what function do I send this command to?

If the CTLE equalizer is a secondary function to the Reference Rx operator, address the :SPRocess:CTLequalizer:FZP command to the Reference Rx function as identified in the following Reference Rx Setup dialog's operator diagram. In the following figure, this would be Function 2 and the command would be:

:SPRocess2:CTLequalizer:FZP

Requires FlexDCA revision A.06.60 and above.