:SPRocess:CTLequalizer:PRESets:SELections?
Query Syntax
:SPRocessN:CTLequalizer:PRESets:SELections?
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Query Response
"preset name, preset name, preset name, …"
Description
Returns a string which is a comma-separated list of all saved presets for the Continuous Time Linear Equalizer (CTLE) operator. Use the PRESet command to load one of these presets.
For Reference Rx operator, what function do I send this command to?
If the CTLE equalizer is a secondary function to the Reference Rx operator, address the :SPRocess:CTLequalizer:PRESets:SELections command to the Reference Rx function as identified in the following Reference Rx Setup dialog's operator diagram. In the following figure, this would be Function 2 and the command would be:
:SPRocess2:CTLequalizer:PRESets:SELections
CTLE Operator Presets
- IEEE 802.3dj Draft 2.0
- IEEE 802.3ck
- CEI-112G-Linear (53GBd)
- CEI-112G-VSR-PAM4 (56GBd)
- CEI-112G-VSR-PAM4 (58GBd)
- IEEE 802.3bs CDAUI-8 (1 dB)
- IEEE 802.3bs CDAUI-8 (1.5 dB)
- IEEE 802.3bs CDAUI-8 (2 dB)
- IEEE 802.3bs CDAUI-8 (2.5 dB)
- IEEE 802.3bs CDAUI-8 (3 dB)
- IEEE 802.3bs CDAUI-8 (3.5 dB)
- IEEE 802.3bs CDAUI-8 (4 dB)
- IEEE 802.3bs CDAUI-8 (4.5 dB)
- IEEE 802.3bs CDAUI-8 (5 dB)
- IEEE 802.3bs CDAUI-8 (5.5 dB)
- IEEE 802.3bs CDAUI-8 (6 dB)
- IEEE 802.3bs CDAUI-8 (6.5 dB)
- IEEE 802.3bs CDAUI-8 (7 dB)
- IEEE 802.3bs CDAUI-8 (7.5 dB)
- IEEE 802.3bs CDAUI-8 (8 dB)
- IEEE 802.3bs CDAUI-8 (8.5 dB)
- IEEE 802.3bs CDAUI-8 (9 dB)
- CEI-56G-VSR-NRZ (1dB)
- CEI-56G-VSR-NRZ (2dB)
- CEI-56G-VSR-NRZ (3dB)
- CEI-56G-VSR-NRZ (4dB)
- CEI-56G-VSR-NRZ (5dB)
- CEI-56G-VSR-NRZ (6dB)
- CEI-56G-VSR-NRZ (7dB)
- CEI-56G-VSR-NRZ (8dB)
- CEI-56G-VSR-NRZ (9dB)
- CEI-56G-VSR-NRZ (10dB)
- CEI-56G-VSR-NRZ (11dB)
- CEI-56G-VSR-NRZ (12dB)
- OIF CEI-28G-VSR (0dB)
- OIF CEI-28G-VSR (1dB)
- OIF CEI-28G-VSR (2dB)
- OIF CEI-28G-VSR (3dB)
- OIF CEI-28G-VSR (4dB)
- OIF CEI-28G-VSR (5dB)
- OIF CEI-28G-VSR (6dB)
- OIF CEI-28G-VSR (7dB)
- OIF CEI-28G-VSR (8dB)
- OIF CEI-28G-VSR (9dB)
Requires FlexDCA revision A.04.50 and above.