:SPRocess:CTLequalizer:DEFinition

Instrument:
N1000A
N109x
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Package License:
L-RND

Command Syntax

:SPRocessN:CTLequalizer:DEFinition {POLE2 | POLE3 | GAIN2}

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function. The following table lists the child commands available for the three CTLE definitions.

Query Syntax

:SPRocessN:CTLequalizer:DEFinition?

Query Response

{POLE2 | POLE3 | IEEE}

Description

Specifies the type of Continuous Time Linear Equalizer (CTLE) operator. You can select a 2 pole CTLE (POLE2), a 3 pole CTLE (POLE3), or a CTLE based on the IEEE 802.3ck standard (GAIN2). The following tables show the valid child commands for configuring the CTLE based on the CTLE's definition as set by this command. Be sure to look at the available factory presets that can be selected with :CTLequalizer:PRESet. To configure the filter's Aliased Noise Processing, use the :SPRocess:CTLequalizer:PNOise command.

Before selecting the type of CTLE, send the :FUNCtion:FOPerator CTLE command to first create the operator.

Commands Available for Defining a CTLE Operator
Child Commands Description CTLE Definition Argument
POLE2 POLE3 GAIN2
:SPRocess:CTLequalizer:DEFinition Selects type of CTLE ■ ■ ■
:SPRocess:CTLequalizer:GAIN DC gain ■ ■
:SPRocess:CTLequalizer:GAIN:NORMalize Turns DC gain on or off ■ ■
:SPRocess:CTLequalizer:GDC Low frequency gain (Gdc and Gdc2) ■
:SPRocess:CTLequalizer:ZERo Zero frequency ■ ■ ■
:SPRocess:CTLequalizer:FZP Low-frequency zero/pole ■
:SPRocess:CTLequalizer:POLe Pole frequency ■ ■ ■
:SPRocess:CTLequalizer:PNOise Noise processing ■ ■ ■
:SPRocess:CTLequalizer:PRESets Recall and save CTLE settings as preset ■ ■ ■

For Reference Rx operator, what function do I send this command to?

If the :CTLE equalizer is a secondary function to the Reference Rx operator, address the :SPRocess:CTLequalizer:DEFinition command to the Reference Rx function as identified in the following Reference Rx Setup dialog's operator diagram. In the following figure, this would be Function 2 and the command would be:

:SPRocess2:CTLequalizer:DEFinition

Requires FlexDCA revision A.06.60 and above.

This command replaces deprecated command :SPROcess:CTLequalizer:PCOunt.