:SPRocess:CTLequalizer:GDC

Instrument:
N1000A
N109x
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Package License:
L-RND

Command Syntax

:SPRocessN:CTLequalizer:GDC{1|2} <low-frequency gain>

<low-frequency gain> is a double.

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:SPRocessN:CTLequalizer:GDC?

Description

The :SPRocess:CTLequalizer:GDC1 form of this command specifies the low frequency gain (Gdc) applied by an IEEE based CTLE operator. The gain is specified in dB. You can also set the Zero frequency (:SPRocess:CTLequalizer:ZERo), the Low-Frequency Zero/Pole (:SPRocess:CTLequalizer:FZP), and Pole frequency (:SPRocess:CTLequalizer:POLe). For Gdc2, send the :SPRocess:CTLequalizer:GDC2 form of the command. Before selecting this command, send the :FUNCtion:FOPerator CTLE command to first create the operator followed by :SPRocess:CTLequalizer:DEFinition IEEE to define the type of CTLE.

 

Commands Available for Defining a CTLE Operator
Child Commands Description CTLE Definition Argument
POLE2 POLE3 GAIN2
:SPRocess:CTLequalizer:DEFinition Selects type of CTLE ■ ■ ■
:SPRocess:CTLequalizer:GAIN DC gain ■ ■
:SPRocess:CTLequalizer:GAIN:NORMalize Turns DC gain on or off ■ ■
:SPRocess:CTLequalizer:GDC Low frequency gain (Gdc and Gdc2) ■
:SPRocess:CTLequalizer:ZERo Zero frequency ■ ■ ■
:SPRocess:CTLequalizer:FZP Low-frequency zero/pole ■
:SPRocess:CTLequalizer:POLe Pole frequency ■ ■ ■
:SPRocess:CTLequalizer:PNOise Noise processing ■ ■ ■
:SPRocess:CTLequalizer:PRESets Recall and save CTLE settings as preset ■ ■ ■

For Reference Rx operator, what function do I send this command to?

If the CTLE equalizer is a secondary function to the Reference Rx operator, address the :SPRocess:CTLequalizer:GDC command to the Reference Rx function as identified in the following Reference Rx Setup dialog's operator diagram. In the following figure, this would be Function 2 and the command would be:

:SPRocess2:CTLequalizer:GDC

Requires FlexDCA revision A.06.60 and above.