:SPRocess:RANDom:JITTer:RMS
Instrument:
N1000A
N109x
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Package License:
L-RND
Command Syntax
:SPRocessN:RANDom:JITTer:RMS <jitter>
<jitter> is a double.
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Query Syntax
:SPRocessN:RANDom:JITTer:RMS?
Description
Specifies the amount of random jitter, in seconds, applied by a Random operator. To learn how specify the amount of random noise applied, refer to the :SPRocess:RANDom:NOISe:SPECtrum command.
Requires FlexDCA revision A.06.60 and above.
This command is equivalent to (but replaces) deprecated command :SPROcess:RANDom:JITTer.