:SYSTem:MPButton:DOCWizard:BFName
Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:SYSTem:MPButton:DOCWizard:BFName "<filename>"
"<filename>" is a string of the file name including an optional path. The string can include path substitution strings.
Query Syntax
:SYSTem:MPButton:DOCWizard:BFName?
Description
When the Multi-Purpose button is configured to documentation wizard file, this command identifies the path and name of the saved file. The default file (including path) is:
%USER_DATA_DIR%\Documentation Results\DocumentationResults.zip
To configure the Multi-Purpose button to save a documentation wizard file, use the :SYSTem:MPButton:FUNCtion command.
Example Command Sequence
:SYSTem:MPButton:DOCWizard:BFName "%USER_DATA_DIR%\Documentation Results\DocWizard.zip" :SYSTem:MPButton:FUNCtion SDWFile
Requires FlexDCA revision A.04.50 and above.