:SYSTem:MPButton:SIMage:MONochrome
Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:SYSTem:MPButton:SIMage:MONochrome {ON | OFF}
Query Syntax
:SYSTem:MPButton:SIMage:MONochrome?
Description
Turns monochrome screen capture on and off. When on, a black and white image will be saved. Selecting monochrome automatically inverts the graticule area's background color. When off, you can invert the graticule area's background color using the :INVert sibling command. To configure the Multi-Purpose button to save a screen image to a file, use the :SYSTem:MPButton:FUNCtion command.
Requires FlexDCA revision A.04.50 and above.