:SYSTem:MPButton:SIMage:INVert
Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:SYSTem:MPButton:SIMage:INVert {ON | OFF}
Query Syntax
:SYSTem:MPButton:SIMage:INVert?
Description
Turns on and off the inversion of the graticule area's background color. The entire application window is saved with a black graticule upon a white background. The waveform colors remain unchanged. Inversion is automatically turned on and cannot be turned off if the :MONochrome sibling command is enabled. To configure the Multi-Purpose button to save a screen image to a file, use the :SYSTem:MPButton:FUNCtion command.
Requires FlexDCA revision A.04.50 and above.