:TDR:DESKew:CONTinue
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Command Syntax
:TDR:DESKew:CONTinue
Description
When the TDR Step Deskew Wizard has paused for user input, use this command to continue the wizard. Use the :TDR:DESKew:CANCel command to abort the wizard. Use the :TDR:DESKew:STARt command to start the TDR Step Deskew Wizard.
Requires FlexDCA revision A.04.00 and above.