:TDR:DESKew:DUT
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Command Syntax
:TDR:DESKew:DUT DUTN
Where N indicates one of 16 possible DUT setups. For example, :DUT4.
Query Syntax
:TDR:DESKew:DUT?
Description
Selects the DUT setup on which to perform a step deskew using the TDR Step Deskew Wizard. If only one DUT setup has been created, it is not necessary to use this command. Use the :TDR:DESKew:STARt command to start the TDR Step Deskew Wizard.
Requires FlexDCA revision A.04.00 and above.
Example Command Sequence
:TDR:DESKew:DUT DUT2 :TDR:DESKew:STARt :TDR:DESKew:SDONe? :TDR:DESKew:CONTinue *OPC?