:TDR:DESKew:STARt
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Command Syntax
:TDR:DESKew:STARt
Description
Starts the TDR Step Deskew Wizard that compensates for unequal TDR step paths to the measurement reference plane. For each channel, step skew and software delay are measured as needed. To manually enter TDR skew values, use the :TDR:STIMulus:CHANnel:SKEW command. If you will be performing a TDR calibration, you do not need to perform a TDR fixture deskew. The TDR calibration fully deskews the steps in addition to compensating the response of your fixture. If you are making TDT measurement and you are using a receiver module, such as an N1045A, to make these measurements, refer to the :TDR:DESKew:SCHannel command.
Requires FlexDCA revision A.04.00 and above.
Example Command Sequence
:CHAN2A:DISPlay ON :CHAN2B:DISPlay ON :TDR:DESKew:DUT DUT2 :TDR:DESKew:STARt :TDR:DESKew:SDONe? :TDR:DESKew:CONTinue :TDR:DESKew:SDONe? :TDR:DESKew:SAVE ON :TDR:DESKew:FNAMe "DUT2 deskew.setx :TDR:DESKew:CONTinue