:TDR:DESKew:SAVE
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Command Syntax
:TDR:DESKew:SAVE {ON | OFF}
Query Syntax
:TDR:DESKew:SAVE?
Description
Turns on and off the saving of a TDR deskew to a file. Use the :TDR:DESKew:FNAMe command to specify the name of the saved file. Use the :TDR:DESKew:STARt command to start the TDR Step Deskew Wizard. The deskew compensates for unequal TDR step paths to the measurement reference plane. Use the :TDR:DESKew:STARt command to start the TDR Step Deskew Wizard.
Requires FlexDCA revision A.04.00 and above.