:TDR:DESKew:SDONe?
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Query Syntax
:TDR:DESKew:SDONe?
Description
Queries the TDR Step Deskew Wizard to determine if the wizard has paused for user input or has completed. Use an *OPC (Operation Complete) command to notify the calling application that the wizard is ready to respond. Use the :TDR:DESKew:STARt command to start the TDR Step Deskew Wizard.
Use of an *OPC? query to pause program execution while waiting for this command to execute.
Requires FlexDCA revision A.04.00 and above.
Example Command Sequence
:TDR:DESKew:DUT DUT2 :TDR:DESKew:STARt :TDR:DESKew:SDONe?;*OPC? :TDR:DESKew:CONTinue *OPC?