:TDR:SPMemory:CLEar

Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
TDR
Waveform type:
S-Parameter
Package License:
L-SNT
L-MFG

Command Syntax

:TDR:SPMemory{1:8}:CLEar

Where the {1:8} specifier identifies one of eight S-parameter memories.

Description

Clears all S-parameters from the selected S-parameter memory. There is no command to clear all S-parameter memories. Instead, issue this command once for each of the four memories.

Requires FlexDCA revision A.05.00 and above.

Example Command

:TDR:SPMemory2:CLEar