:TDR:SPMemory:ENABle?

Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
TDR
Waveform type:
S-Parameter
Package License:
L-SNT
L-MFG

Query Syntax

:TDR:SPMemory{1:8}:ENABle?

Where the {1:8} specifier identifies one of eight S-parameter memories.

Description

Queries the selected memory to determine if S-parameter data has been loaded into it. Returns a '1' if the memory contains data and returns a '0' if it does not contain data.

Requires FlexDCA revision A.05.00 and above.

Example Command

:TDR:SPMemory3:ENABle?