:TDR:SPMemory:DSTatus:REASon?
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
TDR
Waveform type:
S-Parameter
Package License:
L-SNT
L-MFG
Query Syntax
:TDR:SPMemory{1:8}:DSTatus:REASon?
Where the {1:8} specifier identifies one of eight S-parameter memories.
Query Response
<string>
Description
Returns a description of the status of the specified S-parameter memory. If S-parameter data are currently in the specified S-parameter memory location, the name of the source waveform will be returned. For example, "Source: Channel 1A". If the S-parameter memory is empty, the string "Please select a file." is returned. If the file is corrupt or an incorrect type, the string "Unable to load file." is returned. To check the status of the S-parameter memory, use the :TDR:SPMEMory:DSTatus? parent query.
Requires FlexDCA revision A.05.70 and above.
Example Command
:TDR:SPMemory2:DSTatus:REASon?