:TDR:SPMemory:FILE:LOAD
Command Syntax
:TDR:SPMemory{1:8}:FILE:LOAD
Where the {1:8} specifier identifies one of eight S-parameter memories.
Description
Loads an S-parameter file into the destination S-parameter memory. Use the :TDR:SPMemory:FILE:NAME command to specify the name of the S-parameter file to load. All S-parameters contained in the file will be loaded into the S-parameter memory. The default folder for S-parameter files is %USER_DATA_DIR%\S-Parameter Data. S-parameter memory is available in TDR/TDT, Eye/Mask, and Oscilloscope modes. It is not available in Jitter mode.
To load into memory all currently available S-parameters from another S-parameter memory or from a DUT in TDT/TDT mode, use the :TDR:SPMemory:LOAD command.
When importing S-parameters from a file, the frequency spacing in the file must be uniform or the file will not be loaded into memory.
Requires FlexDCA revision A.05.70 and above.
Example Command
:TDR:SPMemory3:FILE:LOAD