:TDR:SPMemory:DSTatus?
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
TDR
Waveform type:
S-Parameter
Package License:
L-SNT
L-MFG
Query Syntax
:TDR:SPMemory{1:8}:DSTatus?
Where the {1:8} specifier identifies one of eight S-parameter memories.
Query Response
{CORR | INV}
Description
Returns the status of the specified S-parameter waveform memory. Up to four memories are available. To query the reason for the current state of the memory, use the :TDR:SPMemory:DSTatus:REASon? query. The following responses can be returned:
CORR- The S-parameter memory location contains S-parameter data. To clear memory, use the
:TDR:SPMemory:CLEarcommand. INV- The S-parameter memory location does not contain data.
Requires FlexDCA revision A.05.70 and above.
Example Command
:TDR:SPMemory2:DSTatus?