:TIMebase:PTIMebase:RFRequency
Instrument
N1000A-PTB
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
Jitter
Command Syntax
:TIMebase:PTIMebase:RFRequency <clock rate>
<clock rate> is a double.
Query Syntax
:TIMebase:PTIMebase:RFRequency?
Description
Specifies the frequency of the reference clock at the N1000A-PTB front-panel internal Precision Timebase Input. The N1000A-PTB precision timebase input requires a full or sub-rate reference clock signal (square wave, BERT output, or a sine wave) from 2.4 to 44 GHz. If pattern lock is turned on, you can turn on autodetection of the reference clock using using the :PTIMebase:RFRequency:AUTo command. If the instrument is unable to correctly detect the external reference frequency, turn autodetection off and manually enter the rate.
PRBS data is not a suitable reference clock signal.
Requires FlexDCA revision A.03.00 and above.