:TIMebase:PTIMebase:RFRequency:AUTo
Instrument
N1000A-PTB
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
Jitter
Command Syntax
:TIMebase:PTIMebase:RFRequency:AUTo {ON | OFF}
Query Syntax
:TIMebase:PTIMebase:RFRequency:AUTo?
Description
Enables or disables automatic detection of the reference clock rate at the N1000A-PTB front-panel internal Precision Timebase Input. Automatic detection occurs during an Auto Scale (:SYSTem:AUToscale). If the instrument is unable to correctly detect the reference rate, turn autodetection off and manually enter the rate using the :TIMebase:PTIMebase:RFRequency command.
Automatic detection requires that pattern lock be turned on.
Requires FlexDCA revision A.03.00 and above.