:TIMebase:PTIMebase:STATe

Instrument
N1000A-PTB
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
Jitter

Command Syntax

:TIMebase:PTIMebase:STATe {ON | OFF}

Query Syntax

:TIMebase:PTIMebase:STATe?

Query Response

{1 | 0}

Description

Enables and disables the N1000A-PTB internal precision timebase. Enabling the precision timebase also sets the time reference. Disabling the precision timebase invalidates the time reference.

N1060A. Inserting an N1060A module into an N1000A-PTB mainframe disables the N1000A-PTB precision timebase and sets the :TIMebase:PTIMebase:STATe SCPI command to OFF. In this situation, only the N1060A's precision timebase can be used.

To control an N1060A module's internal precision timebase, use commands found in the :PTIMebase subsystem. Refer to :PTIMebase:STATe.

Requires FlexDCA revision A.03.00 and above.

Example Command Sequence

:TIMebase:PTIMebase:STATe ON