:TIMebase:PTIMebase:VPTBsignals
Instrument
N1000A-PTB
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
Jitter
Command Syntax
:TIMebase:PTIMebase:VPTBsignals {ON | OFF | 1 | 0}
Query Syntax
:TIMebase:PTIMebase:VPTBsignals?
Description
Turns on and off the display of the two precision timebase IQ input waveforms. These two waveforms are displayed on the Precision Timebase tab, which is located on Setup dialogs for the N1000A-PTB internal precision timebase option. To return the waveforms to the computer, use the :WAVeform:SOURce command. The query form of the command returns the current display state, on or off.
Requires FlexDCA revision A.05.30 and above.