:TIMebase:PTIMebase:RTReference
Instrument
N1000A-PTB
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
Jitter
Command Syntax
:TIMebase:PTIMebase:RTReference
Description
Resets the N1000A-PTB Internal Precision Timebase option. If the time reference fails to set, an error is produced. The usual causes for not being able to set the time reference include missing, too small, or too large signal or a frequency that is not in the specified ranges.
Requires FlexDCA revision A.03.00 and above.