:TRIGger:SRATe

Instrument
N1000A-PLK
N1092x-PLK
N1093A/B-PLK
N1094A/B-PLK
Meas. mode:
Scope
Eye
Jitter
Flex Apps:
FlexDCA
FlexRT

Command Syntax

:TRIGger:SRATe  <symbol rate>

<symbol rate> is a double.

Query Syntax

:TRIGger:SRATe?

Description

When using pattern lock use this command to enter or read the symbol rate of the trigger source. Automatic detection must be turned off before the entered symbol rate setting is applied (:TRIGger:SRATe:AUTodetect).

Requires FlexDCA revision A.05.60 and above.

This command replaces deprecated command :TRIGger:BRATe.

Example Command Sequence

:TRIGger:SRATe:AUTodetect OFF
:TRIGger:SRATe 2.0E+10