:TRIGger:RSYMbol:AUTodetect
Instrument
N1000A-PLK
N1092x-PLK
N1093A/B-PLK
N1094A/B-PLK
Meas. mode:
Scope
Eye
Jitter
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:TRIGger:RSYMbol:AUTodetect {ON | OFF | 1 | 0}
Query Syntax
:TRIGger:RSYMbol:AUTodetect?
Description
Automatically determines the reference symbol for the pattern and aligns the timebase with the reference symbol. The location is selected based on the longest run of symbols with a preference for lowest-level symbols. The pattern at the reference symbol is aligned to the display's left edge. To realign the timebase to use the left edge of the screen as the reference symbol for the pattern use the :TRIGger:RSYmbol:SCTimebase command.
To determines the reference symbol for DCA-M modules that have triggering capability, use the :SLOT subsystem's :SLOT:TRIGger:RSYMbol:AUTodetect command.
Requires FlexDCA revision A.06.71 and above.
This command replaces deprecated command :TRIGger:PALign.