86100D Regulatory Information and Instrument Markings
86100A Regulatory Information
To find a current Declaration of Conformity for a specific Keysight product, go to:
http://www.keysight.com/go/conformity
SAFETY: Complies with the essential requirements of the European Low Voltage Directive as well as current editions of the following standards (dates and editions are cited in the Declaration of Conformity):
- IEC/EN 61010-1
- Canada: CSA C22.2 No. 61010-1
- USA UL std no. 61010-1
EMC
Complies with the essential requirements of the European EMC Directive as well as current editions of the following standards (dates and editions are cited in the Declaration of Conformity):
- IEC/EN 61326-1
- CISPR Pub 11 Group 1, Class A
- AS/NZS CISPR 11
- ICES/NMB-001
This ISM device complies with Canadian ICES-001.
Cet appareil ISM est conforme a la norme NMB-001 du Canada.
South Korean Class A EMC Declaration:
This equipment is Class A suitable for professional use and is for use in electromagnetic environments outside of the home.
Instrument Markings
The following table lists the definitions of markings that may be on the instrument.