JSA RJ (rms) Measurement

Instrument:
N1000A
N107x-JSA
N1060A-JSA
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
Jitter
Package License:
L-RND
L-SNT
Waveforms:
NRZ
PAM4

The JSA RJ (rms) measurement is a band-limited Random Jitter measurement. Specify the integration limits using the Jitter Spectrum Analysis Setup dialog.

JSA requires an N1076A or N1077A module. To use JSA in Jitter Mode, Feature F-JSA is required.

SCPI Command

:MEASure:CRECovery:RJ?

:MEASure:JSAMemory:RJ?