JSA TJ (rms) Measurement
Instrument:
N1000A
N107x-JSA
N1060A-JSA
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
Jitter
Package License:
L-RND
L-SNT
Waveforms:
NRZ
PAM4
The JSA TJ (rms) measurement is a band-limited Total Jitter measurement. Specify the integration limits using the Jitter Spectrum Analysis Setup dialog.
JSA requires an N1076A or N1077A module. To use JSA in Jitter Mode, Feature F-JSA is required.
SCPI Command
:MEASure:CRECovery:TJ?
:MEASure:JSAMemory:TJ?