<CLimitLineTestData> Element
Instrument
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
TDR
<CLimitLineTestData> is the required root element and must be the first element in any Limit Line Test file. This element is the ancestor of all other elements. This element should immediately be followed by the <CLimitLine> element which draws a limit line.
Parent Elements
None.
Child Elements
<CLimitLine> and <CLimitLinePoint> (descendant)
Attributes
| Name | Value | Description |
|---|---|---|
| Name | string | Optional attribute which names a Limit Line Test in the Limit-Line Results table. |
Example
<CLimitLineTestData Name="Compliance Test"> <!-- Define Upper Limit Line --> <CLimitLine Name="top rail" IsMaxLine="True"> <CLimitLinePoint X="0" Y="150e-03" /> <!-- Define the first point --> <CLimitLinePoint X="500e-12" Y="150e-03" /> <!-- Define another point --> <CLimitLinePoint X="600e-12" Y="400e-03" /> <!-- Define another point --> <CLimitLinePoint X="900e-09" Y="400e-03" /> <!-- Define another point --> </CLimitLine> <!-- Finish the line --><!-- Define Lower Limit Line --> <CLimitLine Name="bottom rail" IsMaxLine="False"> <CLimitLinePoint X="0" Y="-150e-03" /> <CLimitLinePoint X="500e-12" Y="-150e-03" /> <CLimitLinePoint X="600e-12" Y="-400e-03" /> <CLimitLinePoint X="900e-09" Y="-400e-03" /> </CLimitLine> </CLimitLineTestData>