<CLimitLinePoint> Element
Instrument
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
TDR
<CLimitLinePoint> defines a limit line point (X,Y) that establishes the beginning or end of a limit line segment. Points within a limit line must be defined in ascending order of X values. The only exception is when two consecutive points have the same X value, as when creating a vertical limit line segment between two segments having different amplitudes. Any number of adjacent points can have the same Y value. The maximum number of points in a limit line is 2048, which results in 2047 limit line segments. If points are not defined in ascending X values, the file will fail to load and an error will be reported.
Time and amplitude values are interpreted to be in the window's current vertical and horizontal units.
Parent Elements
Child Elements
None.
Attributes
| Name | Value | Description |
|---|---|---|
| X | string | Sets the point's time. |
| Y | string | Sets the point's amplitude. |
Example
<CLimitLineTestData Name="Compliance Test"> <!-- Define Upper Limit Line --> <CLimitLine Name="top rail" IsMaxLine="True"> <CLimitLinePoint X="0" Y="150e-03" /> <!-- Define the first point --> <CLimitLinePoint X="500e-12" Y="150e-03" /> <!-- Define another point --> <CLimitLinePoint X="600e-12" Y="400e-03" /> <!-- Define another point --> <CLimitLinePoint X="900e-09" Y="400e-03" /> <!-- Define another point --> </CLimitLine> <!-- Finish the line --><!-- Define Lower Limit Line --> <CLimitLine Name="bottom rail" IsMaxLine="False"> <CLimitLinePoint X="0" Y="-150e-03" /> <CLimitLinePoint X="500e-12" Y="-150e-03" /> <CLimitLinePoint X="600e-12" Y="-400e-03" /> <CLimitLinePoint X="900e-09" Y="-400e-03" /> </CLimitLine> </CLimitLineTestData>