:JOBS:CONFig:LDEFinition?
Flex Apps:
FlexOTO
FlexOTO Instance:
Stations
Query Syntax
:JOBS:CONFig:LDEFinition? <Job ID>
Where <Job ID> is an integer that represents the Job ID.
Query Response
{RLMA120 | RLMC94 | EYE}
Description
For specified Job ID, returns the Linearity Definition setting, which based on one of the following standards:
- RLMA120
- RLM (IEEE 802.3 Annex 120D). This is the default definition.
- RLMC94
- RLM (IEEE 802.3 Clause 94)
- EYE
- Eye Linearity (CEI 4.0)
The units can be set to dBM (DBM) or Watts (WATT). The default setting is Watts.