:JOBS:CONFig:TMPReset?
Flex Apps:
FlexOTO
FlexOTO Instance:
Stations
Query Syntax
:JOBS:CONFig:TMPReset? <Job ID>
Where <Job ID> is an integer that represents the Job ID.
Query Response
"<preset-name>"
For example, "IEEE 802.3cd". Notice that the response includes double quotes.
Description
For specified Job ID, returns the TDECQ Measurement Preset for the associated fixture's Lane. For example, "IEEE 802.3cd". To return the fixture name and Lane number, pass the same Job ID to the :JOBS:CONFig:FIXTure? and :JOBS:CONFig:LANE? queries.
| IEEE 802.3bs |
| IEEE 802.3bs Amended |
| IEEE 802.3cd (Covers the IEEE 802.3cu clause) |
| IEEE 802.3db/D2.0 |
| Fiber Channel PI - 7 Rev 0.13 |
To change the TDECQ Measurement Preset for an existing Test Program line, use :TPRogram:SLINe:TMPReset.
When creating a Test Program, enter the TDECQ Measurement Preset with :TPRogram:SETup:TMPReset.