:JOBS:CONFig:MEASurements?
Flex Apps:
FlexOTO
FlexOTO Instance:
Stations
Query Syntax
:JOBS:CONFig:MEASurements? <job-id>
Where <Job ID> is an integer that represents the Job ID.
Query Response
"[APOW,][CEQ,][CROS,][CD,][EDIM,][ERAT,][LIN,][NONE,][OER,][OMAX,][OOMA,][OVER,][PPP,][TDEC,][TDEQ,][TTIM,][UND,][VECP,][WDAT]"
Description
For specified Job ID, returns the comma separated string of the FlexOTO measurements performed. For example,
TDEQ,OER,OVER,UND
If the Job ID is for a user measurement (Instrument), the query returns NONE. This query can respond anytime after a Test Program has been started. The Job ID's Job Results do not have to be completed before this query can return a valid response. The following string values represent the measurements:
APOW- Average Power measurement.
CEQ- Ceq measurement.
EDIM- Eye diagram graphics file. The eye diagram image has been selected to be saved for this Job ID. To return the image data using a binary transfer, use the
:JOBS:RESults:SIMage?query. To save the image in a zip file, use the:DISK:RESults:SAVEcommand. The graphics file is named EyeDiagram_N.png where N identifies the Job ID. Don't confuse this save with the:DISK:SIMage:SAVEcommand which saves an image of FlexOTO's GUI. NONE- Response from a Job ID for a measurement performed on a user Instrument.
OER- Outer Extinction Ratio measurement.
OOMA- Outer OMA measurement.
OVER- Overshoot measurement.
PPP- Peak-Peak Power measurement.
TDEQ- Transmitter and Dispersion Eye Closure (TDECQ) measurement.
TTIM- Transition Time measurement.
UND- Undershoot measurement.
WDAT- PAM4 Waveform Data. Waveform data has been selected to be saved for this Job ID. Waveform files can be imported into FlexDCA's waveform memory. To save the data in a zip file, use the
:DISK:RESults:SAVEcommand. The Waveform file is named Waveform_N.png where N identifies the Job ID.