:JOBS:CONFig:PUNits?
Flex Apps:
FlexOTO
FlexOTO Instance:
Stations
Query Syntax
:JOBS:CONFig:PUNits? <Job ID>
Where <Job ID> is an integer that represents the Job ID.
Query Response
{DBM | WATT}
Description
For the specified Job ID, returns the power units that are used for the following measurements. The returned units can be dBm (DBM) or Watts (WATT). The default setting is Watts. All of these measurements, if present, are set to the same unit of measurement. If you want the unit to be different for, say Average Power, configure your Test Program so that Average Power is on a separate line than the remaining three measurements. This results in a unique Job ID, and so units selection, for the Average Power measurement.
The affected measurements are:
- Outer OMA
- Average Power
- Peak-Peak Power measurements
- Transmitter Power Excursion
To configure a Test Program line's power units, use the command or :TPRogram:SETup:PUNits:TPRogram:SLINe:PUNits command.