:JOBS:CONFig:CRPReset?
Flex Apps:
FlexOTO
FlexOTO Instance:
Stations
Query Syntax
:JOBS:CONFig:CRPReset? <Job ID>
Where <Job ID> is an integer that represents the Job ID.
Query Response
"<preset-name>"
For example, "IEEE 802.3bs/cd/ck (53 GBd)". Note that the response includes double quotes.
Description
For specified Job ID, returns the Clock Data Recovery (CDR) Preset for the associated fixture's Lane. For example, "5.312500000E+10". To return the fixture name and Lane number, pass the same Job ID to the :JOBS:CONFig:FIXTure? and :JOBS:RESults:LANE? queries.
To change the CDR Preset for an existing Test Program line, use :TPRogram:SLINe:CRPReset.
When creating a Test Plan, enter the CDR Preset with :TPRogram:SETup:CRPReset.