:JOBS:CONFig:PLENgth?
Flex Apps:
FlexOTO
FlexOTO Instance:
Stations
Query Syntax
:JOBS:CONFig:PLENgth? <Job ID>
Where <Job ID> is an integer that represents the Job ID.
Description
For specified Job ID, returns the pattern length for the associated fixture's Lane. For example, "5.312500000E+10". To return the fixture name and Lane number, pass the same Job ID to the :JOBS:CONFig:FIXTure? and :JOBS:CONFig:LANE? queries.
To change the pattern length for an existing Test Program line, use :TPRogram:SLINe:PLENgth.
When creating a Test Program, enter the pattern length with :TPRogram:SETup:PLENgth.