:JOBS:CONFig:TEPRest?
Flex Apps:
FlexOTO
FlexOTO Instance:
Stations
Query Syntax
:JOBS:CONFig:TEPReset? <Job ID>
Where <Job ID> is an integer that represents the Job ID.
Query Response
"<preset-name>"
For example, "IEEE 802.3cd". Notice that the response includes double quotes.
Description
For specified Job ID, returns the TDECQ EQ Preset for the associated fixture's Lane. For example, "IEEE 802.3cd". To return the fixture name and Lane number, pass the same Job ID to the :JOBS:CONFig:FIXTure? and :JOBS:CONFig:LANE? queries.
To change the TDECQ EQ Preset for an existing Test Program line, use :TPRogram:SLINe:TEPReset.
When creating a Test Program, enter the TDECQ EQ Preset with :TPRogram:SETup:TEPReset.