:JOBS:CONFig:ERUNits?
Flex Apps:
FlexOTO
FlexOTO Instance:
Stations
Query Syntax
:JOBS:CONFig:ERUNits? <Job ID>
Where <Job ID> is an integer that represents the Job ID.
Query Response
{DEC | PERC | RAT}
Description
For the specified Job ID, returns the ER units that are used for the Outer ER measurement. The returned units can be set to decibel (returns DEC), percent (returns PERC), or ratio (returns RAT). The default setting is decibel.
To configure a Test Program line's power units, use the command or :TPRogram:SETup:ERUNits:TPRogram:SLINe:ERUNits command.