:JOBS:CONFig:THRatio?
Flex Apps:
                                                FlexOTO
                                            FlexOTO Instance:
                                                Stations
                                            Query Syntax
:JOBS:CONFig:THRatio? <Job ID>
Where <Job ID> is an integer that represents the Job ID.
Query Response
<hit_ratio> is a double.
Description
For specified Job ID, returns the Target Hit Ratio setting which is used in overshoot and undershoot measurements. The default hit ratio is 0.01 which is called out in the IEEE 802.3cu standard. The minimum value is 0.0. The maximum value is 0.1.