:JOBS:CONFig:FIXTure?
Flex Apps:
FlexOTO
FlexOTO Instance:
Stations
Query Syntax
:JOBS:CONFig:FIXTure? <job-id>
Where <Job ID> is an integer that represents the Job ID.
Query Response
"<fixture-name>"
Where <fixture-name> is a string that identifies the name of the Fixture block on the switch diagram.
Description
For specified Job ID, returns the name of the fixture being tested. The name identifies the fixture block on the Hardware Diagram and is listed in the Job Results panel. To rename the fixture, send :CONFigure:FIXTure:REName to FlexOTO Hardware Diagram.
This query can respond anytime after the Test Program has started. The Job ID's Job Results do not have to be completed before this query can return a valid response.