Clock Generator Block Setup
FlexOTO Instance:
Hardware Diagram
Use the Clock Gen Setup dialog to rename a Clock Generator block. Clock Generator blocks represent a test setup clock that is common to multiple DUT fixtures. This clock can be directly connected to the Clock In port on an N1092-series DCA-M rather than performing clock recovery.
Place Clock Generator blocks to the right side of the Switch block in the Hardware Diagram.
| Hardware Diagram Clock Gen Block | Clock Gen Setup Dialog |
|---|---|
|
|