:RMEMory Subsystem
The :RMEMory (Response Memory) subsystem allows you to load previously saved Response files (.rspx) into any of the four Response Memories and to clear data from a memory. You can also change the manner in which a Response Memory's plots (JTF, JTF modeled, and OJTF modeled) are displayed. This includes turning the display of the plots on or off, changing their color, or giving the response memory plots a custom name. To configure Response plots, use the commands in the :RESPonse subsystem.
Use the :RMEMory:FILE:LOAD command to load a Response file into a Response Memory. To find out if a Response Memory is empty, use the :RMEMory:AVAilable command. Use the :RMEMory:CLEar command to clear the data from a selected memory thus making the memory available. To display the Response that is loaded in memory, use the :RMEMory:DISPlay command.
In addition, the commands under the :RMEMory:PLLModel node select whether the PLL loop settings for calculating the Response Memory models are automatically or manually selected (:RMEMory:PLLModel:ALOop:ENABle). When manually selected, use the following commands to configure the settings:
- Loop Gain (
:RMEMory:PLLModel:MLOop:FGAin) - Loop Zero (
:RMEMory:PLLModel:MLOop:FZERo) - Loop Pole (
:RMEMory:PLLModel:MLOop:FPOLe)